This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: System Halt issue

Part Number: AM3358

I'm having an issue with certain custom boards with the AM3358 processor halting.I can't get any message using serial. The AM3358 is running in 1Ghz.

When the AM3358 running, I measure the voltage of VDD_MPU and VDD_CORE. VDD_MPU‘s peak to peak voltage is as high as 330mV, minimum voltage 1.137V, maximum voltage 1.473V, exceeding the datasheet requirements of 1.272-1.378V.

 Is the range(1.272V-1.378V) Vpp, ripple or rms?