This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Blackhawk XDS560v2-USB Mezzanine Emulator仿真器连接c6678开发板报错

使用c6678开发平台;

Blackhawk XDS560v2-USB Mezzanine Emulator仿真器;

 CCS: 5.2.1.00018;

仿真器相关配置如下:

测试连接的时候打印错误日志如下,麻烦帮忙分析一下,好多谢!

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\DOCUME~1\ADMINI~1\LOCALS~1\APPLIC~1\.TI\
213602635\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'Aug 30 2012'.
The library build time was '22:16:38'.
The library package version is '5.0.838.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the Nano-TBC VHDL.
The link is a 560-class second-generation-560 cable.
The software is configured for Nano-TBC VHDL features.
The controller will be software reset via its registers.
The controller has a logic ONE on its EMU[0] input pin.
The controller has a logic ONE on its EMU[1] input pin.
The controller will use falling-edge timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '2' (0x0002).
The utility logic has not previously detected a power-loss.
The utility logic is not currently detecting a power-loss.
Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

[End]

  • 这块EVM板之前能连上仿真器么,还是一直连不上,截个图上来看看你是怎么连的,注意在上电后过个几分钟等等仿真器启动后再连接仿真器。

  • Andy Yin1,您好:

                   之前是一直用可以连接仿真器的,连接方法是用BiosMulticoreSDK_2.1_GettingStartedGuide.pdf讲述的方法:

    而上述打印信息是我点击Test Configuration 测试连接的打印信息:

    在Test Configuration测试连接的时候还有可能打印消息如下:

    [Start]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\DOCUME~1\ADMINI~1\LOCALS~1\APPLIC~1\.TI\
    213602635\0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'bh560v2u.out'.
    Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc
    The library build date was 'Aug 30 2012'.
    The library build time was '22:16:38'.
    The library package version is '5.0.838.0'.
    The library component version is '35.34.40.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '5' (0x00000005).
    The controller has an insertion length of '0' (0x00000000).
    The cable+pod has a version number of '8' (0x00000008).
    The cable+pod has a capability number of '7423' (0x00001cff).
    This utility will attempt to reset the controller.
    This utility has successfully reset the controller.

    -----[Print the reset-command hardware log-file]-----------------------------

    The scan-path will be reset by toggling the JTAG TRST signal.
    The controller is the Nano-TBC VHDL.
    The link is a 560-class second-generation-560 cable.
    The software is configured for Nano-TBC VHDL features.
    The controller will be software reset via its registers.
    The controller has a logic ONE on its EMU[0] input pin.
    The controller has a logic ONE on its EMU[1] input pin.
    The controller will use falling-edge timing on output pins.
    The controller cannot control the timing on input pins.
    The scan-path link-delay has been set to exactly '2' (0x0002).
    The utility logic has not previously detected a power-loss.
    The utility logic is not currently detecting a power-loss.
    Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc

    An error occurred while hard opening the controller.

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver or utilities.

    The value is '-230' (0xffffff1a).
    The title is 'SC_ERR_PATH_MEASURE'.

    The explanation is:
    The measured lengths of the JTAG IR and DR scan-paths are invalid.
    This indicates that an error exists in the link-delay or scan-path.

    [End]

  • 我们也遇到了同样问题,DSP上电后,检测checkout时钟是否正确,正确的话,内核应该工作正常,JTAG口烧坏

    更换新的DSP,jtag做保护,连接正常

  • 请教一下,用的板子是C6678,但是和pc了解是总是没反应,应该是驱动没有安装成功。请问驱动是否可以单独安装?

  • 请问这个问题怎么解决呀
x 出现错误。请重试或与管理员联系。