This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm3730 dsp encode问题

Other Parts Discussed in Thread: OMAP3530, DM3730

dear all:

我现在在dm3730上调试dsp h264encode,现在使用的omap3530的encode程序,

现在发现encode 60秒时间文件大小差不多有24M,1小时的话要1G多,

请问这个h264编码是不是没有进过压缩?文件怎么会这么大?

PS 摄像头数据是PAL制720X576,30帧左右?

                                         望知道的高手指导下,谢谢

  • 你好,

    请问24M是b还是B?编码应该可以设定目标码率的,是以每秒多少bit来计算的。如果是24MB,码率也即是24x8/60=3.2Mbps。60秒的原始数据的大小是720x576x2x30x60=1492992000B~=1493MB。

    D1 30f/s设定1Mbps的码率时候图像质量应该就不错了。

  • hello Chris,

    我把码率设置为1Mbps,现在1分钟大约10MB左右,1小时600M,

    请问这个大小还可以继续优化不?

    另外,VIDENC1_Params中的maxFrameRate = 30,maxInterFrameInterval =1;

    VIDENC1_DynamicParams中的refFrameRate =30,targetFrameRate = 30,intraFrameInterval = 30,这些参数修改会改善编码后的文件大小么?

    D1 30f/s 可是打印出来的信息video fps却是42,这是为什么?

    谢谢