This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs3.3 printf() 函数没有输出?

工程已经添加了库 rts32earm9.lib ,并设置堆栈大小都是0x1000

printf() 函数始终无法输出

  • 包含了stdio.h头文件么?
    #include <stdio.h>

  • 另外,你有没有用DSP/BIOS?

  • 添加了 #include <stdio.h>,也没有使用DSP/BIOS

    把文件贴出来看看:

    CMD文件

    -e _boot

    IRAMStart = 0x80000000;
    IRAMSize = 0x00020000;

    DDRStart = 0xc0000000;
    DDRSize = 0x04000000;

    DRAMStart = 0x80000000;
    _DRAMSize = 0x00020000;

    STACKStart = IRAMStart + IRAMSize;

    _NAND_EMIFStart = 0x62000000;
    _NOR_EMIFStart = 0x60000000;

    MEMORY
    {
    ARM_INTERNAL_RAM (RWXI): origin = 0x80000000 length = 0x0001FFFF
    SDRAM (RWXI): org=0xc0000000 length = 0x02000000
    }

    SECTIONS
    {
    .boot: load = 0x80000000
    .text: load > ARM_INTERNAL_RAM
    .data: load > ARM_INTERNAL_RAM
    .bss: load > ARM_INTERNAL_RAM
    }

    入口文件:

    extern void boot( void ) __attribute__((naked,section(".boot")));

    void boot(void)
    {
    asm(" .global STACKStart");
    asm(" .global _stack");
    asm(" .global main");
    asm(" NOP");
    asm(" MRS r0, cpsr");
    asm(" BIC r0, r0, #0x1F"); // CLEAR MODES
    asm(" ORR r0, r0, #0x13"); // SET SUPERVISOR mode
    asm(" ORR r0, r0, #0xC0"); // Disable FIQ and IRQ
    asm(" MSR cpsr, r0");
    asm(" NOP");

    // Set the IVT to low memory, leave MMU & caches disabled
    asm(" MRC p15,#0,r0,c1,c0,#0");
    asm(" BIC r0,r0,#0x00002300");
    asm(" BIC r0,r0,#0x00000087");
    asm(" ORR r0,r0,#0x00000002");
    asm(" ORR r0,r0,#0x00001000");
    asm(" MCR p15,#0,r0,c1,c0,#0");
    asm(" NOP");

    // Setup the stack pointer
    asm(" LDR sp,_stack");
    asm(" SUB sp,sp,#4");
    asm(" BIC sp, sp, #7");

    // Call to main entry point
    main();

    asm("_stack:");
    asm(" .word STACKStart");
    }

    请指点一下到底哪里有问题?

  • 没看到调用printf函数的语句,不过我猜是没有在结尾加\n的原因。