This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 SmartReflex 如何设置

Other Parts Discussed in Thread: UCD9222, UCD7242

我的电源采用UCD9222+ucd7242给c6778的cvdd供电,用FUSION软件设置输出电压为1.1V,为什么我测量输出电压为1.1v为固定电压,c6678没有调节它呢?smartreflex通过VID应该根据情况会调节输出的。

  • 你可以在DSP上电时用示波器看一看VID的输出是什么,到硬件设计手册里查这个VID对应的电压是多少,如果是111110左右,那么就是要求输出1.1V。

    如果VID和UCD输出对应不上,那么建议你去电源的版面咨询一下如何调整。

x 出现错误。请重试或与管理员联系。