This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 里面的SWM模块如何指定具体的实例(如SC5 SC1..)



由于某种原因我使用的RDK版本较低,dec_display 的demo无法使用标清播放,我想在想自己添加模块改成能够支持标清的,但是在设置swM模块的参数时,一直看不懂如下几行(在MultiCh_Vdec_Vdis.c中)

#if defined(TI_814X_BUILD) || defined(TI_8107_BUILD)

{

swMsPrm[0].numSwMsInst = 2;

swMsPrm[0].swMsInstId[0] = SYSTEM_SW_MS_SC_INST_VIP1_SC;
swMsPrm[0].swMsInstId[1] = SYSTEM_SW_MS_SC_INST_SC5;

swMsPrm[0].swMsInstStartWin[0] = 0;
swMsPrm[0].swMsInstStartWin[1] = 10;

}

#else

省略。

    我想问下这里面的swMsPrm[0].numSwMsInst =2 是如何确定的,SYSTEM_SW_MS_SC_INST_VIP1_SC和 SYSTEM_SW_MS_SC_INST_SC5是如何指定的。

在附下一张linkapi的链接图: