This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求OMAPL138可以自举的bin代码



大家好,不知谁可以帮忙写个OMAPL138arm端小代码:

使OMAPL138的GPIO6[0]、GPIO6[2]间断输出高低电平(即2个led闪烁),使用你们认为可以norflash模式启动的方式,使用的ais格式的bin文件(aisgen工具中为16bit、CS2 0x60000000、clock晶振为24MHZ、cpu 300MHZ、其他配置为常用的即可),(norflash启动使用ais格式,暂不用table或image的,因为后来复杂代码需要)。(我用的是CCSv3.3,如果有正对这个版本的工程更好,不是的话也没关系)

我想试试在我现在用的板子上能否运行?您的这种方式是否可以自举?

我的代码现在一直自举不成功,我也写了简易测试led的代码,仿真器测试都是可以的,就是自举不成功,所以我想参考大家各种norflash启动的方式,万分感谢!!

1245715504@qq.com