This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用6657LS

Other Parts Discussed in Thread: BIOSLINUXMCSDK

1,我在创建引导表的时候,readme.text文档中说道。在 Generating the program to create an IBL binary中,

Now edit the file device.c

- There are individual functions for each EVM supported in the release. Edit the appropriate function. If multiple EVMs/SOCs are going to be used, then it is better to make the changes for each EVM at this stage

2,Then issue the command

  cd ibl/src/util/iblConfig/build这个有事需要我在cmd中打开什么呢?build里面没有他要的东西啊、

然后他又说C6657
make EVM=c6670l I2C_MAP_ADDR=0x500  这个是文档的错误吗?明明是6657的,为什么在make evm上确实显示6670?

求专家指点1,2.

  • 你是在编译IBL么,你用的mcsdk是什么版本,建议下载安装最新的版本。IBL的编译及使用在mcsdk_2_01_02_06\tools\boot_loader\ibl\doc下面有指导。

    mcsdk下载路径:http://www.ti.com/tool/bioslinuxmcsdk