我用的是6678的开发板,现在需要通过PCIe接口加载引导程序,在哪可以找到相关的例程?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在6678的bootloader的源代码中,有这样一个宏定义:#define DEVICE_REG_BOOT_PROGRESS *((volatile unsignedint *)0x02620140) 但是我在DataManual上查0x02620140的寄存器定义发现地址0x02620140为Reserved,并且在函数中确实用到了此寄存器来进行了处理(例如在函数void chipSetBPField(UINT 32 value,UINT32 msb,UINT32 lsb)中),我想问此寄存器有什么作用,并且在TI有没有6678的所有寄存器一览表什么的?
PCIe一次初始化配置就可以了
可以利用TI提供的CSL库进行配置
在最新的MCSDK安装路径下mcsdk_install_path\tools\boot_loader\examples可以学习PCIe的配置