我查看了AR0330+DM368IPC 的CVBS信号输出,发现图像内容只有通过网络传输的1920*1080P 图像的1/9左右,也就是只有屏幕中央位置1/9左右的图像。请问,可以设置为同网络输出一样视野宽度的CVBS信号吗?也就是可否设置为高清视频像素隔点采样输出?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我查看了AR0330+DM368IPC 的CVBS信号输出,发现图像内容只有通过网络传输的1920*1080P 图像的1/9左右,也就是只有屏幕中央位置1/9左右的图像。请问,可以设置为同网络输出一样视野宽度的CVBS信号吗?也就是可否设置为高清视频像素隔点采样输出?
你好,
可以使能RSZB输出D1,然后把这个D1送给CVBS输出。但是这样会增加DDR的访问,对系统性能可能会有影响。
Chris Meng 您好:
我将DM365/8数据手册都搜索遍了,也找不到RSZB ; 这个关键词,以及RSZB与您所说D1的关联,
请您进一步说明,好吗? 万分感激!