我C6678通过AMC转PCie连接,在PCIe接口上挂接了PCIe转SATA芯片,请问在c6678的内存中如何能找到该芯片的DEVID和VENID????我找完了从0x21800000 开始的32K地址空间都找不到。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我C6678通过AMC转PCie连接,在PCIe接口上挂接了PCIe转SATA芯片,请问在c6678的内存中如何能找到该芯片的DEVID和VENID????我找完了从0x21800000 开始的32K地址空间都找不到。
你可以查看Vendor and Device Identification Register 寄存器,TI 提供的PCle 接口 VENID都是0x104C
另外你说看不到,是从DSP memory中看不到,还是RC侧看不到?
谢谢回复,现在能够找到dsp的PCIe的ID,0x8888104C,我希望找的是我PCIe转SATA的控制芯片的ID,该芯片为祥硕的asm1061,ID为1b21 0612 如果把PCIe配置成RC模式的话,我想应该在 SUBSYS_VNDR_ID寄存器中应该可以查看到该芯片的ID吧,可是该寄存器的值一直为0x00010000,意思就是说RC模式下的PCIe模式没能识别到该芯片,如何才能识别该芯片呢????,求教,谢谢!