This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678多核编组同时运行后不响应IPC中断



Core0为主核,Core1-Core5为从核,各从核依次运行后可以正常响应主核的IPC中断。但将Core1-Core5编组同时运行后就不能响应主核的IPC中断了,请问可能是什么原因?

从核的main函数内依次是:

Bootcfg_unlockkicker();

init_interrupt();

while(1);

  • void interrupt_init()
    {
    intcContext.eventhandlerRecord = EventHandler;
    intcContext.numEvtEntries = 30;
    CSL_intcInit(&intcContext);
    CSL_intcGlobalNmiEnable();
    CSL_intcGlobalEnable(&state);
    vectId = CSL_INTC_VECTID_6;
    hTest = CSL_intcOpen(&intcObj, 91, &vectId, NULL);
    //Register an call-back handler which is invoked when the event occurs.
    EventRecord.handler = &IPC_service;
    EventRecord.arg = 0;
    CSL_intcPlugEventHandler(hTest, &EventRecord);
    CSL_intcHwControl(hTest, CSL_INTC_CMD_EVTENABLE, NULL);
    }

  • 问题已解决,原因是Bootcfg_unlockkicker();函数的问题。

    只保留一个Bootcfg_unlockkicker函数即可解决问题。

  • 你好!我目前在做多核加载,需要主核向从核发送IPC中断来启动从核。我在主核的main程序开始向IPCGR1中写入0x1,来启动核1,现在是从核1一直处于idle状态,不能正确启动,我查了一下原因,是IPC中断没有写进去。请问在主核的main程序中向从核写IPC中断前,要不要做中断初始化。如果需要,该如何初始化,有没有初始化代码?