This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6713外扩DM9000移植lwip,数据发送速率略慢



在TI的6713B上面移植协议栈作为TCP服务器成功了,但是数据发送速度不是特别快,一秒内发送72Byte的数据包为2000个,我设置的TCP_MSS 72*20,其它的如tcp_snd_buf 4*mss等等,另外,我测试了一下就是不经过lwip协议栈,在主函数里面直接调用DM9000_send函数来发送数据(没有按照tcp、ip数据格式),大概一秒钟也就300个包,不过发送的这个包大小在(1B-3kB)之间,希望各路大神能不吝指教。分析了一下可能是因为DM9000发送函数里面处理的比较慢,解决办法暂时没有想到,另外一个解决思路是我通过协议栈一次发送大于1460个数据包(但是苦于不知道怎么实现),跪求大神解答啊