This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM6678

Other Parts Discussed in Thread: CDCE62005, TMDXEVMPCI

各位好!

我将EVM6678插入三个主机进行了测试,遇到一些问题想问一下,希望能有人给出建议。

1.我将评估板EVM6678插入第一个台主机,采用的是PCIE启动方式,薄码开关设置为

     SW3(off,on,on,off)

    SW4(on,on,on,on)

    SW5(on,on,on,off)

    SW6(off,on,on,on)

此时主机无法检测到硬件,通过寄存器发现0x21800004的值为6,而LTSSM_STATE为0x00. 手动将LTSSM_EN改为1,此时LTSSM_STATE为0x11,即正常状态。但是在“设备管理器”下面却看不到设备,这是为什么?

2.EVM6678的PCIE reference clock的时钟是谁提供的?是通过PCIE卡槽提供的还是通过芯片提供的?

3.EVM6678是否有用到PERST这个复位信号?如果有,那么是怎么用的?

4.将EVM6678插入第二个PC机上,该PC能正确枚举EVM6678,加载同样的驱动程序也没问题,EVM6678能和主机正常进行通信。而将EVM6678(同样的配置)插入第三个PC机上,该主机能够枚举到EVM6678,但是装驱动的时候直接黑屏重启,请问这种情况是为什么?

希望有人能给出建议,谢谢!

  • 没有人能回答一下上面的问题吗?大牛们帮帮忙呗

  • EVM6678的PCIE reference clock的时钟默认是由EVM板上的时钟芯片(CDCE62005)提供,但也可以通过调整控制时钟片选的FPGA由AMC输入提供

    PERSET 没有用到

    请问你三个PC的主板型号是否一样,另外你的安装是否遵循如下顺序

                    a. Please upgrade to latest IBL available from MCSDK 2.0 GA, by following steps specified in tools\boot_loader\ibl\doc\evmc66xx-instructions.txt. Please ensure to use “swap_data = 0” in tools\writer\eeprom\evmc66xxl\bin\eepromwriter_input.txt when you perform step 1 of “Programming IBL on the EEPROM at bus address 0x51”.

                    b. Please set C667x EVM to PCIE boot mode. Please refer tools\boot_loader\examples\pcie\docs\readme.pdf to learn how to set this boot mode.

                    c. Power off ATX chassis and Disconnect power cord of ATX chassis

                    d. Insert TMDXEVMPCI with C667xL/LE EVM into ATX chassis. There must not be any external power supply connected to C667xL/LE EVM.

                    e. Connect power cord to ATX chassis and power on ATX chassis.

                    f. For Linux Users: Enter “lspci” command, a C667xL/LE EVM will detect as “Multimedia controller” in list of PCI devices, as shown in below figure with RED box.

                       For Windows Users: Go to Device Manager, you can see new Hardware detected as “Multimedia Controller” as shown in below figure with RED box.

  • 您好!

    谢谢您的回复!

    我用的是三个不同的主板进行的测试,安装也按照您说的顺序了,但是还是出现问题。

    在第一个主板(研华Q35)上,EVM6678能正常工作。EVM6678没进行任何修改,插入另外两台测试机(一个是研祥Q67,另一个是研华的Q77)的时候一安装驱动程序就黑屏重启。

    您对这种情况有什么建议吗?希望您能给出一点思路,谢谢!

  •  ,您好!

        我个人理解应该是EVM6678插入另外两台PC机后,并没有分配到资源,即主机BIOS自检过程只识别了硬件,却没分配资源给该硬件。如果是这样,那我想问一下造成这种现象的可能原因会是什么?(我用的是TI给的IBL,并没有进行任何修改)

        您能回复一下吗?谢谢!