This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730不能从SD卡启动

Other Parts Discussed in Thread: DM3730, TPS65930, OMAP3530

电路参考DM3730的开发板devkit5800D连接方式,刚刚贴片回来,三块板子相同故障现象如下:

1.TPS65930三个核心电压1.2V 1.2V和1.8V输出正常,VMMC1电压输出为0,;

2.boot脚配置没问题,26M和32K时钟输出正常;

3.插上SD卡后串口没有打印信息,稳压源输出电流大小无变化,推断DM3730没有启动;

4.给VMMC1连接一个外部3.3V,现象仍是如此,不能启动;

以前使用OMAP3530时由于I2C4连接错误,TPS65930也是没有VMMC1电压输出,外接一个3.3V电压后可以从SD卡启动的,但是DM3730却是不行,哪位能给点思路,这个问题折腾很久了。