所使用DSP为TMS320VC5410A,仿真环境:CCS3.3。
进入CCStudio v3.3,打开示例程序,编译通过,再选择File->Load Program时,出现如下错误提示:
Trouble Writing Register:
Error 0x80001024/-1058
Fatal Error during: Register, Execution, Target,
Device driver: Emulator Controller not responding
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
之后选择Disconnect,再选择Debug->Reset Emulator,再选择Debug->Connect,就出现下列错误提示:
Trouble Reading Memory Block at 0xff7d on Page 0 of Length 0x27:
Error 0x80000002/-1058
Fatal Error during: Memory,
Device driver: Emulator Controller not responding
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
请问上述问题是硬件设计问题吗?如果不是,又是什么问题呢?该如何解决上述问题?