This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PIN MUX about UART0_PRUSS1 & MDIO_PRUSS1

Other Parts Discussed in Thread: TLK110

1.使用pin mux 配置了6个串口UART0,UART1,UART2,UART3,UART4,UART0_PRUSS1(仅支持rx,tx)

  问题:这样的配置在资源上能否满足6个UART的要求?另外UART0_PRUSS1和其余UART0~5有什么区别吗?

2. 硬件配置了RMII1和RMII2,和MDIO_PRUSS1

 问题:这样的配置和两片TLK110连接有问题没?MDIO_PRUSS1和MDIO有区别吗?

附件为配置文件,请问这样的配置有问题嘛?

PinMuxDesignState_AM335x Rev 2.x.dat
  • 不是很建议你如此设计,理由有

    (1)你只是用到UART, MDIO,因为而用上带PRU的AM335X,增加成本,同时,PRU的UART,MDIO操作起来,至少在软件驱动上会略有区别。

    (2)两个网口都用起来的情况下,MDIO可以共用,详细可以参考starterkit的设计。

  • 是否可以这样理解,如果不具备PRU功能的AM335x,

        其管脚UART0_PRUSS1,不可以配置成UART功能

                   MDIO_PRUSS1, 不可以配置成MDIO功能

                   MII0_PRUSS1 管脚不可以配置成MII功能等;