在6670开发板上跑mcsdk 里面的BCP例程 C:\ti\pdk_C6670_1_1_2_6\packages\ti\drv\exampleProjects 主要跑的LTE pdsch ,出现以下输出:
[C66xx_0] **************************************************
*************** BCP Example Start ****************
**************************************************
Using BCP Driver version: 0x1000100 Version Info: BCP Driver Revision: 01.00.01.00:Nov 19 2012:16:11:43
[Core 0]: L1D cache size 0. L2 cache size 0.
[Core 0]: BCP instance 0 successfully initialized
[Core 0]: BCP driver successfully opened
Global FDQ 877 successfully setup with 256 descriptors
-------------- LTE DL Test Start --------------
Rx FDQ 736 successfully setup with 62 descriptors
Flow 0 opened to send data to RxQ: 900
Tx FDQ 737 successfully setup with 2 descriptors
Error reading test vectors/populating packet
LTE DL Test: FAILED
-------------- BCP Testing Complete --------------
Num Test Failures = 1
**************************************************
****************** BCP Example End ***************
**************************************************
[Core 0]: BCP Example Unloaded successfully
BcpAlloc Cnt: 67 BcpFree Cnt: 66
CppiMalloc Cnt: 1 CppiFree Cnt: 0
QmssAlloc Cnt: 0 QmssFree Cnt: 0