初学SRIO,准备用论坛上提供的keystone_SRIO 这个工程中的SRIO_2DSP_Test来实现两个6678DSP之间的通信。积攒了一些问题,请各位专家不吝赐教~~
1.每个DSP的rapidIO是不是就只有一个DEVICE ID,还是4个通道每个通道都可以有一个?为什么会有16个可选的deviceID呢? main()函数中 srio_cfg.device_ID_routing_config = dsp0(1)_device_ID_routing_config,是不是在这里设定了每个设备的地址?SRIO_2DSP_Test()中的
Keystone_SRIO_match_ACK_ID()是用来检测相应port的链路是否建立成功,函数参数DSP1_SRIO_BASE_ID,与dsp1_device_ID_routing_config那个结构体有 什么联系?
2.On Turbo Nyquist EVM only lane 2 and 3 are connected between 2 DSPs,如果我的两个DSP全部4通道都相连,是不是仿照2,3作相应修改就ok了?
3.只想用的DirectIO 的 SRIO_PKT_TYPE_SWRITE 模式,是不是最大一次的uiByteCount可以是1M?
4.我想实现两个DSP相互通信,而不是只是DSP0 master负责发,DSP1 slave负责收,是不是把DSP1仿照DSP0那样配置,而不是主函数里else后面的配置就可以实现这样的功能?
谢谢各位~