大家好!
6678 & ccs 5.3
我在板子上跑ndk的两个demo,client和helloworld,在dhcp模式下跑的时候,console输出如下:
[C66xx_0] QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
TCP/IP Stack Example Client
Configuring DHCP client
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Verify_Init: Expected 0 entry count for Queue number = 911, found 1 entries
Verify_Init: Expected 0 entry count for Queue number = 913, found 1 entries
Registration of the EMAC Successful, waiting for link up ..
Service Status: DHCPC : Enabled : : 000
Service Status: Telnet : Enabled : : 000
Service Status: HTTP : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
我在mcsdk user guide中看到有一张运行的界面图,它在输出enable running之后,会输出Network Added If xx.xx.xx.xx 这样的ip信息,但我的一直没有出现,所以感觉是一直没有被分到ip
我看到有些帖子中提到要一个dhcp server(我看到pc上有一个DHCP Client的服务),我试着下了一个dhcp server,但不怎么有用。
请问这个问题怎么解决呢?还是说需要做一些什么配置吗?
谢谢!