This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于EDMA的link问题



各位专家好!

EDMA在进行link传输的时候,交替加载两组参数通过一个通道进行传输,我现在设置了一个源地址和两个目的缓冲区,交替往两个目的缓冲区传送数据,我希望的是在往第一个缓冲区传输完数据后,将源缓冲区剩下的数据继续往另一个缓冲区传送,结果发现往第一个缓冲区传输完数据以后,EDMA又将源地址的数据全部的往第二个缓冲区传送了一遍,而不是希望的那样讲源地址剩下的数据传送到第二个缓冲区,请问是什么原因呢?如果要达到希望的效果,应该做些什么修改?谢谢!

#include <stdio.h>

#include <string.h>

#include <ti/csl/csl_edma3.h>

#include <ti/csl/csl_edma3Aux.h>

#include "Keystone_common.h"

#include "Keystone_EMIF16_init.h"

/* Global Buffers (Source and Destination) for PING-PONG */

// ping/pong的源缓冲区和目的缓冲区

Uint8 srcBuff[512];

Uint8 dstBuff1[512];

Uint8 dstBuff2[512] 

static Int32 edma_ping_pong_xfer_gbl_region (Int32 instNum, Uint8 channelNum)

{                                           

    CSL_Edma3Handle                 hModule;

    CSL_Edma3Obj                    edmaObj;

    CSL_Edma3ParamHandle            hParamPing;

    CSL_Edma3ParamHandle            hParamPong;

    CSL_Edma3ChannelObj             chObj;

    CSL_Edma3CmdIntr                regionIntr;

    CSL_Edma3ChannelHandle          hChannel;

    CSL_Edma3ParamSetup             myParamSetup;

    CSL_Edma3Context                context;

    CSL_Edma3ChannelAttr            chAttr;

    CSL_Status                      status;

    Uint32                          loopIndex;

    printf ("Debug: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d...\n", instNum, channelNum);

    /* Initialize data数据初始化  */

    for (loopIndex = 0; loopIndex < 256; loopIndex++)

    {

        srcBuff[loopIndex] = loopIndex;

        dstBuff1[loopIndex] = 0;

        dstBuff2[loopIndex] = 0;

    }

    /* Module initialization 模块初始化*/

    if (CSL_edma3Init(&context) != CSL_SOK)

    {

        printf ("Error: EDMA module initialization failed\n");

        return -1;

    }

    /* Open the EDMA Module using the provided instance number使*/

    hModule=CSL_edma3Open(&edmaObj, instNum, NULL, &status);

    /* Channel open*/

    chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL;

    chAttr.chaNum    = channelNum;

hChannel = CSL_edma3ChannelOpen(&chObj, instNum, &chAttr, &status);

    /* Change Channel Default queue setup from 0 to 3  */

   CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_3);

    /* Map the DMA Channel to PARAM Block 2.*/

    CSL_edma3MapDMAChannelToParamBlock(hModule, channelNum, 2);

    /* Obtain a handle to parameter set 2*/

    hParamPing = CSL_edma3GetParamHandle(hChannel, 2, &status);

    /* Obtain a handle to parameter set 1 */

    hParamPong = CSL_edma3GetParamHandle(hChannel, 1, &status);

    /* Setup the parameter entry parameters (Ping buffer) */

    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \

                                             CSL_EDMA3_TCCH_DIS, \

                                             CSL_EDMA3_ITCINT_DIS, \

                                             CSL_EDMA3_TCINT_EN, \

                                             0, CSL_EDMA3_TCC_NORMAL,\

                                             CSL_EDMA3_FIFOWIDTH_NONE, \

                                             CSL_EDMA3_STATIC_DIS, \

                                             CSL_EDMA3_SYNC_A, \

                                             CSL_EDMA3_ADDRMODE_INCR, \

                                             CSL_EDMA3_ADDRMODE_INCR );

    myParamSetup.srcAddr    = (Uint32)srcBuff;

    myParamSetup.aCntbCnt   = CSL_EDMA3_CNT_MAKE(256,1);

    myParamSetup.dstAddr    = (Uint32)dstBuff1;

    myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,1);

    myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);    myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);

    myParamSetup.cCnt = 1;

    /* Ping setup  */

    CSL_edma3ParamSetup(hParamPing,&myParamSetup);

    /* Pong setup 设*/

myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPing,0);

    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \

                                             CSL_EDMA3_TCCH_DIS, \

                                             CSL_EDMA3_ITCINT_DIS, \

                                             CSL_EDMA3_TCINT_EN,\

                                             1, CSL_EDMA3_TCC_NORMAL,\

                                             CSL_EDMA3_FIFOWIDTH_NONE, \

                                             CSL_EDMA3_STATIC_EN, \

                                             CSL_EDMA3_SYNC_A, \

                                             CSL_EDMA3_ADDRMODE_INCR, \

                                             CSL_EDMA3_ADDRMODE_INCR );

    myParamSetup.srcAddr = (Uint32)srcBuff;

    myParamSetup.dstAddr = (Uint32)dstBuff2;

    /* Pong setup  */

    CSL_edma3ParamSetup(hParamPong,&myParamSetup);

    /* Interrupt enable (Bits 0-1)  for the global region interrupts*/

    regionIntr.region = CSL_EDMA3_REGION_GLOBAL;

    regionIntr.intr   = 0x3;

    regionIntr.intrh  = 0x0000;

    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);

    /* Trigger channel */

    CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);

    regionIntr.region = CSL_EDMA3_REGION_GLOBAL;

    regionIntr.intr   = 0;

    regionIntr.intrh  = 0;

    /* Poll on IPR bit 0 */

    do {

        CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);

    } while (!(regionIntr.intr & 0x1));

    /* Clear the pending bit   */

    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,®ionIntr);

    /* Trigger Channel  */

    CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);

    /* Poll on IPR bit 2 */

    do {

        CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);

    } while (!(regionIntr.intr & 0x2));

    /* Close channel */

CSL_edma3ChannelClose(hChannel);

    /* Close EDMA module 关闭EDMA模块*/

    CSL_edma3Close(hModule);

    /* The test passed. */

    return 0;

}

void main (void)

{

    Uint8  channelNum=0;

    Uint8  instNum = 0;

    printf("EDMA testing...\n");

    edma_ping_pong_xfer_gbl_region(instNum, channelNum);

    printf("Debug: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d passed\n", instNum, channelNum);

    printf("EDMA test successful\n");

       return;

}

  • 你好:

    你在设置pong的Parameter的时候,这时的源地址应该和Ping的源地址不一样,需要增加偏移。

  • King Wang

       您好!请问Pong地址的偏移应该根据什么来增加呢?另外,如果源地址的数据比较多,需要进行多次pingpong链接传输,也就是在往pong缓冲区传输完数据以后需要重新链接ping参数,这个时候往ping缓冲区传输的数据的源地址应该和原来不一样了,也会发生偏移,那么最开始设置ping参数的时候怎么做到兼顾这一点呢?谢谢!

  • 您好:

    每个parameter只能存放1组数据,源地址和目的地址应该事先都要预先计算好偏移。

    如果需要一次触发进行3次搬移,那么需要3个parameter,pingpong通常只用于两次链接。

    谢谢!