This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【C6670】CVDD核电压的测量



各位TI工程师好,在配置DDR3之前需要先确定核电压CVDD的大小,根据以前的帖子我找到了相关测量的步骤

如上面两幅图所示,根据VCNTL来测量出VID,再从map里找到对应的CVDD值。

但是VCNTL都是输出,如何让VCNTL[3]进行高低电平翻转,进而测量出VID[5:0]

希望工程师们可以给予解答,非常感谢。

  • VCNTL是输出管脚,上电之后DSP内部会自动按照上述贴出的时序输出相应的VCNTL值,电源控制芯片在获取上述的输出值后根据table1解析得到对应的电压值再反馈供给DSP。