This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

spi1 flash启动问题



 用了一块SST25VF080B-50-4C的spiflash芯片。想把omapl138通过spi1 flash的方式启动。已经通过AISgen_d800k800.exe把.out格式文件转成了ais格式的文件。选择如下:

Device Type: d800k800    ARM

Boot Mode:   SPI1 FLASH

Clock source: Crystal    24

选择了Configure PLL0

并且在Peripheral 中设置 SPI Clock: 10

PLL0 设置为:1, 25, 2, 1, 3, 6

 并且也设置了启动引脚,装置上电后无反应。

是不是有哪个地方遗漏了。

代码绝对没有问题,我已经用仿真器运行过了,也用UART2的启动方式测试过了,都可以,但是SPIFLASH的启动方式就是不行!

另外SPI CLOCK的设置,是不是只要不超过最大值都是可以的?

求教?