假如我把DM6467的启动模式设置为SPI MODE. 请问我能用一个CPU(例如DM365)的SPI 去配置DM6467吗?或者用SPI flash去配置DM6467? 有可行性吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
假如我把DM6467的启动模式设置为SPI MODE. 请问我能用一个CPU(例如DM365)的SPI 去配置DM6467吗?或者用SPI flash去配置DM6467? 有可行性吗?
可行性当然是有但
1. 365 应该没有spi slave的驱动,你自己搞应该比较麻烦
2. 这样启动会很慢,因为必须一个芯片起来再起另外一个芯片。
3. DM365 用什么去起?
之前的方案是用海思的一款芯片通过PCI去启动DM6467,现在想用DM365来代替海思的芯片,来启动DM6467,通过SPI。DM365用nand Flash来启动。如果DM365和DM6467分别用各自的nand Flash启动,然后只是通过SPI通信(DM365是主,DM6467是从)技术难度是不是会降低?谢谢。
m 如果你要用IPNC芯片+DSP的方案的话还是尽快迁移到DM8127吧,从哪个方面说都会方便容易一些。
如果DM365、DM6467各自启动,问题在于DM6467侧的SPI slave驱动是否有。
BR,
Eason