参考了很多帖子,知道了IPCFrames是帧数据,IPCBits是流数据,但是在什么时候用还不是很清楚,能讲解一下吗?比如从NSF_Link到 编码Link, 从编码Link到A8存储,分别该用哪一个呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考了很多帖子,知道了IPCFrames是帧数据,IPCBits是流数据,但是在什么时候用还不是很清楚,能讲解一下吗?比如从NSF_Link到 编码Link, 从编码Link到A8存储,分别该用哪一个呢?
你好,
一般是未压缩的数据用IPCFrame,压缩后(h264enc/jpegenc)的数据用ipcbits。
你好 Chris Meng:
在DVRRDK中,有的时候还会使用IPCOUT,IPCOUT和IPCFrameOUT又有什么区别呢?我的理解是 IPCOUT只能用于 VPSS M3与VIEDO M3的核间通信,这样理解正确吗?非常感谢!
我参考demo_vdec_vdis里面的ipcFrames写了一个新的link但是卡在了swMsLink_drv.c: status == FVID2_SOK : failed处,
并且检测到bufList.numFrames的值一直为0
这是我实现的连接,附件里有log和源码http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/98212.aspx
帮忙看看哪里出了问题,谢谢啦