This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368图像传输的疑惑



小弟刚接触DM368没多久,现在使用FPGA产生逐行数字信号,发送至DM368。DM368设置输入模式为RAW Bayer,数据已成功接收,图像基本正确。但仔细地从抓取的图像数据来看,存在几个问题:

1.当FPAG发送两个相邻像素值差距很大的情况下,例如发送FF 00 。。。或 AA 55。。。打印出的数据并不是实际发送的数据。

2.连续的发送相同的数据时,数据正确;

3.连续的发送渐进的数据时,数据基本正确;但在边界处,如.....FD FE FF 00 01 02.... 中的FF 00处,多出一个EE ,后面少了一个 01 ,变成FD FE FF EE 00 02 03。

4.BT656隔行传输下也会出现这种问题

猜想可能原因是:1.DM368的VPSS中的某个module,使图像smooth化; 2.VPSS中把这种高低数据的变化认作bad pixel 处理?

请各位大神指教!!