This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: GPIO1组的持续控制问题

Part Number: AM5718

操作目的:想让uboot对GPIO1的引脚控制持续到系统运行后被应用程序接管;

为此进行了以下操作:

1# 配置内核dts属性

在gpio1节点下添加 “ti,no-reset-on-init;”;

2# 修改内核源码arch/arm/mach-omap2/omap_hwmod_7xx_data.c

static struct omap_hwmod dra7xx_gpio1_hwmod = {
    .name        = "gpio1",
    .class        = &dra7xx_gpio_hwmod_class,
    .clkdm_name    = "wkupaon_clkdm",
    .flags        = HWMOD_INIT_NO_RESET,//HWMOD_CONTROL_OPT_CLKS_IN_RESET,
    .main_clk    = "wkupaon_iclk_mux",
    .prcm = {
        .omap4 = {
            .clkctrl_offs = DRA7XX_CM_WKUPAON_GPIO1_CLKCTRL_OFFSET,
            .context_offs = DRA7XX_RM_WKUPAON_GPIO1_CONTEXT_OFFSET,
            .modulemode   = MODULEMODE_HWCTRL,
        },
    },
    .opt_clks    = gpio1_opt_clks,
    .opt_clks_cnt    = ARRAY_SIZE(gpio1_opt_clks),
};

以上任一操作均可对GPIO5组的GPIO控制保持,但无法使GPIO1组的控制保持,请问还有什么需要操作或注意的地方吗?