This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

320c6657 cmd文件配置问题



想把程序烧写进dsp,具体应该如何配置cmd文件呢?

我目前调试的cmd如下:

MEMORY
{
 /* Local L2, 0.5~1MB*/
 VECTORS:  o = 0x00800000  l = 0x00000200   /*set memory protection attribitue as execution only*/
 LL2_CODE:  o = 0x00800200  l = 0x0000FE00   /*set memory protection attribitue as execution only*/
 LL2_R_DATA:  o = 0x00810000  l = 0x00008000   /*set memory protection attribitue as read only*/
 LL2_RW_DATA:  o = 0x00818000  l = 0x000fffff   /*set memory protection attribitue as read/write*/

 /* Shared L2 1MB for C6657 */
 SL2:   o = 0x0C000000  l = 0x00080000
 SL2_RW_DATA:  o = 0x18000000  l = 0x00080000   /*remapped SL2, set memory protection attribitue as read/write*/
 
 /* External DDR3, upto 2GB per core */
 DDR3_CODE:  o = 0x80000000  l = 0x01000000   /*set memory protection attribitue as execution only*/
 DDR3_R_DATA:  o = 0x81000000  l = 0x01000000   /*set memory protection attribitue as read only*/
 DDR3_RW_DATA:  o = 0x82000000  l = 0x06000000   /*set memory protection attribitue as read/write*/

}

SECTIONS
{
 vecs        >    VECTORS          //中断向量,掉电保护

 .text           >    SL2          //二进制代码,掉电保护
 .cinit          >    SL2          //全局、静态,掉电保护
 .const          >    SL2
 .switch         >    SL2
 .cio            >    SL2
 .stack          >    LL2_RW_DATA   //堆栈
 GROUP
 {
  .neardata
  .rodata
  .bss
 }   >    LL2_RW_DATA
 .far            >    LL2_RW_DATA
 .fardata        >    LL2_RW_DATA
 .sysmem         >    LL2_RW_DATA
 External_NonCache_Data  >  DDR3_RW_DATA
 platform_lib >   SL2
}

请问要烧写进板子该如何修改?其中 中断向量表 应该放到哪里呢?