This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问swms模块Repeat帧是什么意思?



下面是打印信息

[m3vpss ] *** [SWMS0] Mosaic Statistics ***
[m3vpss ]
[m3vpss ] Elasped Time: 601 secs
[m3vpss ]
[m3vpss ] Output Request FPS : 66 fps (40095 frames)
[m3vpss ] Output Actual FPS : 53 fps (32076 frames)
[m3vpss ] Output Drop FPS : 13 fps (8019 frames)
[m3vpss ] Output Reject FPS : 0 fps (0 frames)
[m3vpss ] Scaling Internal : 14 ms
[m3vpss ] Scaling Internal min : 15 ms
[m3vpss ] Scaling Internal max : 15 ms
[m3vpss ]
[m3vpss ] Win | Window Repeat Drop Recv Que FID Invlid Acc Event Invalid Que Reject Reject Latency OutBufCopy InBufCopy
[m3vpss ] Num | FPS FPS FPS FPS FPS FPS Count (Max/Min) CH Frames Frames Frames Min / Max FPS FPS
[m3vpss ] ---------------------------------------------------------------------------------------------------------------------------
[m3vpss ] 0 | 53 53 0 0 0 0 0 ( 0/255) 0 0 0 19172 / 620567 53 0
[m3vpss ] 1 | 53 0 0 54 53 0 480 ( 3/ 3) 0 0 0 884 / 960 0 0
[m3vpss ]
[m3vpss ]
[m3vpss ] *** [SWMS0] Mosaic Parameters ***
[m3vpss ]
[m3vpss ] Output FPS: 60
[m3vpss ]
[m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Scan | Low Cost | SWMS | Data | Blank |
[m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Fmt | ON / OFF | Inst | Format| Frame |
[m3vpss ] ------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
[m3vpss ] 0 | 0 | 0, 0 | 1920 x 540 | 7680 / 7680 | NON-TILED | 0, 270 | 960 x 540 | 3840 / 0 | NON-TILED | PROGRESSIVE | ON | 0 | 422I | OFF |
[m3vpss ] 1 | 1 | 0, 0 | 1920 x 540 | 4096 / 4096 | NON-TILED | 960, 270 | 960 x 540 | 3840 / 0 | NON-TILED | PROGRESSIVE | ON | 0 | 420SP | OFF |


请问我swms 是两路视频进来,为什么第一路会repeat呢,就像是skip了一样,只出来第一帧数据,后面就没有了,第二路是正常输出显示的;


请帮忙分析一下,谢谢