我的启动过程是把DSP.out 转成boot table的并文件,使用hex6x来转换的 -boot选项
然后在arm上 再以boot table的方式 把对应的data搬到对应的dest,搬移以后对dsp进行reset 和wakeup。
但是发现dsp 没有起来, 我dsp的程序是在L2 ram上运行的, 入口地址是0x0080000,我试着再把L2 ram上的代码出来,就发现读出来的全是0.
但是我查了l138的手册,上面说明的是arm可以访问DSP的这块ram的,请教下是怎么回事呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的启动过程是把DSP.out 转成boot table的并文件,使用hex6x来转换的 -boot选项
然后在arm上 再以boot table的方式 把对应的data搬到对应的dest,搬移以后对dsp进行reset 和wakeup。
但是发现dsp 没有起来, 我dsp的程序是在L2 ram上运行的, 入口地址是0x0080000,我试着再把L2 ram上的代码出来,就发现读出来的全是0.
但是我查了l138的手册,上面说明的是arm可以访问DSP的这块ram的,请教下是怎么回事呢?
//
unsigned int entry_point = 0;
unsigned int SectionLenth =0;
unsigned int SectionAddress;
unsigned int * p_SectionAddress;
unsigned int data;
int i;
//Entry point of DSP .out
printf("Loading DSP .bin \n");
//move code to ram
//get entry point
fread((&entry_point), 4, 1, fPtr);
//
fread((&SectionLenth), 4, 1, fPtr);
do
{
fread((&SectionAddress), 4, 1, fPtr);
p_SectionAddress = (unsigned int * )SectionAddress;
for(i=0;i<(SectionLenth/4);i++)
{
fread((&data), 4, 1, fPtr);
* p_SectionAddress = data;
p_SectionAddress++;
}
fread((&SectionLenth), 4,1, fPtr);
}while(SectionLenth != 0x0);
//校验一次,读取再和文件对比一下
//*(unsigned int *)0x80000000 = 0x12345678;
//data = *(unsigned int *)0x80000000;
//
KICK0Ra = 0x83e70b13; //Open Permissions to SYSCFG Registers
KICK1Ra = 0x95A4F1E0; //(Not required for PG2.0 silicon and above)
//Set DSP boot address vector to entry point of DSP program. This must be aligned to 1KB boundaries
HOST1CFG = entry_point;
//Wake up the DSP
//set PSC0.MDCTL15 to to enable the clocks and all transitioning from the SwRstDisable state to Enable state
CSL_PSC_0_MDCTL_15 = (((CSL_PSC_0_MDCTL_15) & (~ (0x0000001Fu))) | 0x03u);
//set (PSC0.PTCMD) to start the state transition sequence for the DSP module
CSL_PSC_0_PTCMD = (((CSL_PSC_0_PTCMD) & ( ~0x00000002u)) | 0x20u );
//Check GOSTAT[1] bit in (PSC0.PTSTAT) for power transition sequence completion
while((((CSL_PSC_0_PTSTART) & 0x00000002u) >> 1) == 1);
//Wait for the STATE bit in (PSC0.MDSTAT15) to change to 3h.
while( ((CSL_PSC_0_MDSTAT_15) & 0x3F) != 0x3u );
//Write a 1 to the LRST bit in PSC0.MDCTL15 to release the DSP local reset
CSL_PSC_0_MDCTL_15 = ((CSL_PSC_0_MDCTL_15) | 0x00000100u);
//DSP wake
#define SYS_BASE 0x01C14000
#define KICK0Ra *(unsigned int*)(SYS_BASE + 0x038)
#define KICK1Ra *(unsigned int*)(SYS_BASE + 0x03c)
#define HOST1CFG *(unsigned int*)(SYS_BASE + 0x044)
/** @brief Base address of PSC memory mapped registers */
#define CSL_PSC_0_BASE (0x01C10000u)
#define CSL_PSC_0_MDCTL_15 *( volatile Uint32* )( CSL_PSC_0_BASE + 0x0A3C )
#define CSL_PSC_0_PTCMD *( volatile Uint32* )( CSL_PSC_0_BASE + 0x0120 )
#define CSL_PSC_0_PTSTART *( volatile Uint32* )( CSL_PSC_0_BASE + 0x0128 )
#define CSL_PSC_0_MDSTAT_15 *( volatile Uint32* )( CSL_PSC_0_BASE + 0x083c)
//