This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657串口通信问题

Other Parts Discussed in Thread: TMS320C6657

工程师您好:

我们正在使用TMS320C6657开发板进行PC与DSP的串口通信。

运行程序时打印信息显示如下:

 [C66xx_0] Initialize DSP main clock = 100.00MHz/1x10 = 1000MHz

Initialize DDR speed = 50.00MHzx26/1 = 1300.000MTS

macaddress: 00:18:30:04:25:23

0183042523

Required baud rate 38400, effective baud rate 39473! 
 Test successfully!

Sending packet fail, packetNum = 16

No TX descriptor available, send packet fail 
请问工程师能提供一下C6657的串口通信例程吗?我们目前急需,卡在这个问题上了,希望工程师能尽快帮助我们。谢谢!
 Test successfully!

Sending packet fail, packetNum = 16

No TX descriptor available, send packet fail