This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
发这个帖子,主要是想问一下,C6670 NDK中helloworld工程中,在什么位置对以太网链路进行了初始化。比如SGMII serdes PLL、SGMII工作在10M/100M还是1000M的、是auto-negotiation还是强制的设置等等。
在调试NDK helloworld工程时,加断点,当程序执行
do
{
rc = NC_NetStart( hCfg, NetworkOpen, NetworkClose, NetworkIPAddr );
} while( rc > 0 );
正常会打印如下几行信息:
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[C66xx_0] Registration of the EMAC Successful, waiting for link up ..
....等等
感觉这里是对以太网链路进行了初始化,可是怎么搜也搜不到'Ethernet subsystem initialization successfully'这样的文字。
希望得到各位帮助!
你好,为什么我在pdk中找不到platform.c文件 我安装的是BIOS-MCSDK_2.1.2.5 后来我又安装了 BIOS-MCSDK_2.1.2.6 发现也没有这个文件
我运行platform_test_evmc6678l例程 运行到platform_init函数时就会出现
Can't find a source file at "/home/gtbldadm/ti/pdk_C6678_1_1_2_5/packages/ti/platform/evmc6678l/platform_lib/Debug/../src/platform.c"
然后我自己在电脑里也的确找不到这个文件。