This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CCS3.3下面Load Program错误的问题!平台是合纵达的DM6467~



你好!

我在CCS3.3上面创建了工程,准备测试程序!编译和生成都顺利通过。但是在下载程序的时候出现了一下的错误:

Trouble Writing Memory Block at 0x1c12020 on Page 0 of Length 0x4:
Error 0x00000002/-1060
Error during: Memory,
An unknown error prevented the emulator from accessing the processor
in a timely fashion.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.

麻烦帮忙看一下应该怎样去解决!谢谢~