This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问,C6748外接的DDR2的最高运行频率是多少?DSP内核对DDR2的最高存取频率是多少?



我注意到一些开发板的DDR2有DDR2-400/533/800/1066几种速度级别,那么C6748支持的最高和最低DDR2频率是多少呢?上述几种速度级别的都可以使用吗?

DSP内核对DDR2的最高存取频率是多少?我咨询一家板卡商,他们回复说C6748外接的DDR2的最高运行频率是312Mhz,如果这个速度是真的,那么,就是说DSP

对DDR2的存取速度也是312MHz,这对于DSP内核456MHz的最高速度来说,是不是拖累了DSP内核,影响最高性能呢?是否可以使用更高频率的DDR2来改善呢?