This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X XMODEM问题



1:启动时串口中打印的:CCCC是不是由XMODEM发的吗

2:有没有这方面的资料

3:这段程序能不能做修改,因为我是裸跑,我感觉我用不到,我想修改成我它的时间,感觉等时间太长

3:这段程序存放在那儿,我能否自己下载,如何下载,有无下载软件

请TI的大神们回答的细一点,因为我是新手,不要云里雾里,刚入门芯片,好多东西不懂

你们就当我是傻子,我就能看懂了,

  • 1. XMODEM只是个文件传输的协议。启动时串口打印的CCCC,是因为你选择的boot模式中有UART启动。

    2. 你看一下AM335x技术手册的26章Initialization。UART启动的部分在26.1.8.5节

    3. 这段程序是芯片的ROM code,不能更改的。如果你是因为串口启动打印CCCC,导致你觉得启动时间过长,你可以选择不带uart启动的启动序列。参考26.1.5.2.1节,对SYSBOOT pin配置可以配置启动序列。如果你是使用MMC0的SD卡启动的话,你可以选择启动序列中MMC0位于第一位的模式,这样你的板子就能直接从MMC0启动了,不会再经过这个CCC的阶段。