This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMC/SD1接口



请教各位一个问题。我新做了一个OMAPL138的板子,此板上OMAPL138的MMC/SD1接口连接了一个WIFI模块—BL-R8189RM2,我在每个信号线上都上拉了一个51K的电阻,板子启动后怎么都识别不到这个WIFI设备。无奈之下,我把我上一版板子的MMC/SD1接口飞到这一版板子的MMC/SD1接口上,然后用上一版板子上电检测,结果识别到了此WIFI设备(上一版板子上电时,这一版板子并没有上电)。两版PCB的MMC/SD1接口原理图几乎一模一样,除了上拉电阻阻值不同:一个是4.75K,一个是51K。

新版PCB走线没有走等长线,不过线长差距不大(300mil内)。

有没有可能是OMAPL138其他模块的配置影响到了MMC/SD1的使用呢?

请问各位,这是什么原因?谢谢。