This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8186启动报错



下面时报错信息,这个问题如何解决?求各位大神给点意见

0x1a4)

[<c003a308>] (do_one_initcall+0x0/0x1a4) from [<c0097440>] (sys_init_module+0x9c                                                                                                 /0x1bc)

[<c00973a4>] (sys_init_module+0x0/0x1bc) from [<c0044da0>] (ret_fast_syscall+0x0                                                                                                 /0x30)

r7:00000080 r6:00000000 r5:0001b398 r4:400aebe0

---[ end trace 6745665cf0040e10 ]---

notify_send_event failed! status = 0xfffffff3

------------[ cut here ]------------

WARNING: at drivers/dsp/syslink/omap_notify/notify.c:776 notify_send_event+0xd4/                                                                                                 0x26c()

Modules linked in: vpss(+) ipv6

Backtrace:

[<c0048b58>] (dump_backtrace+0x0/0x110) from [<c036b8d8>] (dump_stack+0x18/0x1c)

r7:00000000 r6:c02aa1e0 r5:c04692ef r4:00000308

[<c036b8c0>] (dump_stack+0x0/0x1c) from [<c006bd54>] (warn_slowpath_common+0x54/                                                                                                 0x6c)

[<c006bd00>] (warn_slowpath_common+0x0/0x6c) from [<c006bd90>] (warn_slowpath_nu                                                                                                 ll+0x24/0x2c)

r9:c2f2f0c0 r8:00000001 r7:00000002 r6:00000000 r5:00000009

r4:00000000

[<c006bd6c>] (warn_slowpath_null+0x0/0x2c) from [<c02aa1e0>] (notify_send_event+                                                                                                 0xd4/0x26c)

[<c02aa10c>] (notify_send_event+0x0/0x26c) from [<bf068aa0>] (vps_fvid2_init+0x1                                                                                                 64/0x490 [vpss])

[<bf06893c>] (vps_fvid2_init+0x0/0x490 [vpss]) from [<bf0680c0>] (vps_probe+0x60                                                                                                 /0x160 [vpss])

[<bf068060>] (vps_probe+0x0/0x160 [vpss]) from [<c01e0758>] (platform_drv_probe+                                                                                                 0x20/0x24)

r7:c2400080 r6:bf0767d8 r5:c04b3c28 r4:c04b3c28

[<c01e0738>] (platform_drv_probe+0x0/0x24) from [<c01df6c4>] (driver_probe_devic                                                                                                 e+0xd0/0x190)

[<c01df5f4>] (driver_probe_device+0x0/0x190) from [<c01df7ec>] (__driver_attach+                                                                                                 0x68/0x8c)

r7:c2400080 r6:bf0767d8 r5:c04b3c5c r4:c04b3c28

[<c01df784>] (__driver_attach+0x0/0x8c) from [<c01dee70>] (bus_for_each_dev+0x50                                                                                                 /0x84)

r7:c2400080 r6:bf0767d8 r5:c01df784 r4:00000000

[<c01dee20>] (bus_for_each_dev+0x0/0x84) from [<c01df4e8>] (driver_attach+0x20/0                                                                                                 x28)

r6:bf0767d8 r5:bf0767c4 r4:00000000

[<c01df4c8>] (driver_attach+0x0/0x28) from [<c01de748>] (bus_add_driver+0xb4/0x2                                                                                                 34)

[<c01de694>] (bus_add_driver+0x0/0x234) from [<c01dfb24>] (driver_register+0xb0/                                                                                                 0x13c)

[<c01dfa74>] (driver_register+0x0/0x13c) from [<c01e0a44>] (platform_driver_regi                                                                                                 ster+0x4c/0x60)

r9:c263e000 r8:bf07c000 r7:40037000 r6:0001b398 r5:bf0767c4

r4:00000000

[<c01e09f8>] (platform_driver_register+0x0/0x60) from [<c01e0a78>] (platform_dri                                                                                                 ver_probe+0x20/0x70)

[<c01e0a58>] (platform_driver_probe+0x0/0x70) from [<bf07c030>] (vps_init+0x30/0                                                                                                 x5c [vpss])

r5:bf076b44 r4:00000000

[<bf07c000>] (vps_init+0x0/0x5c [vpss]) from [<c003a3d8>] (do_one_initcall+0xd0/                                                                                                 0x1a4)

[<c003a308>] (do_one_initcall+0x0/0x1a4) from [<c0097440>] (sys_init_module+0x9c                                                                                                 /0x1bc)

[<c00973a4>] (sys_init_module+0x0/0x1bc) from [<c0044da0>] (ret_fast_syscall+0x0                                                                                                 /0x30)

r7:00000080 r6:00000000 r5:0001b398 r4:400aebe0

---[ end trace 6745665cf0040e11 ]---

notify_send_event failed! status = 0xfffffff3

VPSS_CORE : Failed to init fvid2 interface,

vpss: probe of vpss failed with error -22

VPSS_CORE : failed to register ti81xx-vpss driver