This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在片仿真过程中出现Device core was hung和Reading Memory Block?EMAC无法进入中断?



Hi,请教如下问题:首先,在launch C6657.ccxml后,将两个DSP核连接,其后就会出现以下的错误,不知道是什么原因,请问能解决么?若能,请问如何解决该问题呢,最好给出详细点的解决方案。很担心是DSP核坏掉了……

2)另外,其中好像core_1能够正常载程序,并正常运行,但是运行GE工程的时候会发现,虽然我往以太网发送数据了,EMAC好像也能收到,就靠外面的小黄色的灯会闪,但是好像不会进行中断函数里面去,因为我在中断函数一开始就加了puts()函数,但没有任何显示。

3)最后,我想问问,基本上是同样的工程,我昨天晚上测试与PC通信的时候还是好好的没有问题,也没有对工程进行太大的修改,但突然间就变得出现各种好像跟硬件出问题似的问题,设备是否有可能出现问题呢?毕竟设备不正常没办法进行调试。

  • error-1143是在上电之后第一次出现的么,对板卡重新复位一下试试;

    error-1202是在什么时候出现的,此时有运行gel或者对DDR初始化么,其提示是访问ddr memory报的错;

    打个断点看看能不能运行到中断函数中;

    硬件不会那么容易出问题的,大多是软件不稳定或者操作上的问题,你可以试试其他的简单程序看看板卡能否运行正常。