DM365配LCD屏时,因其DCLK最小只能为13MHz,目前4.3"屏DCLK一般都为9MHz。
按厂家建议,可接成RGB565或BT656格式。目前,有支持 RGB565的屏,但未见支持BT656的屏。
看规格书,DM365还支持串口RGB,但又分IronMan Mode,9-Bit IronMan Mode。不知这硬件上如何接?
现在的屏也有支持串口RGB的,不知是否可兼容。
有哪位大侠有用DM365驱动过LCD屏的?指点下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM365配LCD屏时,因其DCLK最小只能为13MHz,目前4.3"屏DCLK一般都为9MHz。
按厂家建议,可接成RGB565或BT656格式。目前,有支持 RGB565的屏,但未见支持BT656的屏。
看规格书,DM365还支持串口RGB,但又分IronMan Mode,9-Bit IronMan Mode。不知这硬件上如何接?
现在的屏也有支持串口RGB的,不知是否可兼容。
有哪位大侠有用DM365驱动过LCD屏的?指点下,谢谢!
你好,
对于9MHz的DCLK,你可以利用Pattern Register来实现。
例如:内部DCLK为27Mhz,利用Pattern Register,3个clock输出一个,这样可以实现9MHz。如果LCD大小是640x480,OSD窗口的大小必须是(640x3)x480,因为三个像素会丢弃两个。
你好,
调整left_margin right_margin是将显示内容放在屏幕的正确位置。和输出时钟无关。