Hi,all
如题,现在使用DCC校正黑电平并发送校正后的参数给DM388后,重新抓取RAW数据再进行黑电平校正时,黑电平的值不为0,想通过ITT进行一下校正,查找问题原因,请问ITT打开DCC抓取的RAW数据时,需要怎样设置才能够正常打开。目前知道ITT抓取RAW数据时是有25600字节的头,但是DCC好像没有。请大家帮忙,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,all
如题,现在使用DCC校正黑电平并发送校正后的参数给DM388后,重新抓取RAW数据再进行黑电平校正时,黑电平的值不为0,想通过ITT进行一下校正,查找问题原因,请问ITT打开DCC抓取的RAW数据时,需要怎样设置才能够正常打开。目前知道ITT抓取RAW数据时是有25600字节的头,但是DCC好像没有。请大家帮忙,谢谢。
你好,
可以的。在ITT里面打开文件时候有header的长度设置,你设置为0试试?
hi,Chris,
header改为0某些模块可以打开,但是AWB选取完文件后,设置相关参数后无法显示选取色块的界面,后续步骤也无法继续进行。黑电平模块是可以使用的。能否帮忙试一下ITT的AWB模块怎样使用DCC抓取的RAW数据。谢谢。
你好,
DCC做AWB校准还有图形显示,我建议仍然使用DCC的AWB做校准。