我新下载的ti-sdk-am335x-evm-07.00.00.00-Linux-x86-Install.bin,使用默认镜像,从SD卡启动,我在烧到SD卡时,没看到有uEnv.txt和uImage文件,把卡插到到BBB后,按住BOOT的键,上电,过一会松开手,LED在狂闪,这样是不是没有从SD卡启动到?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我新下载的ti-sdk-am335x-evm-07.00.00.00-Linux-x86-Install.bin,使用默认镜像,从SD卡启动,我在烧到SD卡时,没看到有uEnv.txt和uImage文件,把卡插到到BBB后,按住BOOT的键,上电,过一会松开手,LED在狂闪,这样是不是没有从SD卡启动到?
如果你没改过BBB中eMMC的启动image,就可以看一下启动后,控制台打印出来的kernel版本号:如果是的BBB的eMMC启动,那个kernel版本是3.8的(印象中是这样)。如果是你做的SDK7.0的Linux SD卡启动了,kernel的版本号是3.12的。通过版本号就知道了。
1. 对于BBB,需要按住s2键,才是从tf卡启动
2. 不需要uEnv.txt,但需要把*.dtb文件copy到fat分区。