This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXL138LCDK的RGB565转RGB888

TMDXL138LCDK的RGB565转RGB888是把565的填充到888的高位,然后用565的高323位补偿888的低位。但是有些开发板又是将565的低323位补偿到888的低位。难道这两种做法效果是一样的吗?显示出的效果有什么区别?请懂图像显示的解释一下

  • 从这个贴子来看,:http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/274416.aspx。 下面的连接是可以的,低位接GND。

    其实低位影响不大了,要深究的话,这种颜色映射还得考虑到显示对像本身。

    NC        ->  B0                     NC        ->  G0                NC        ->  R0

    NC        ->  B1                     NC        ->  G1                NC        ->  R1

    NC        ->  B2                     LCD_D5 -> G2                 NC        ->  R2 

    LCD_D0 -> B3                     LCD_D6 -> G3                 LCD_D11 -> R3

    LCD_D1 -> B4                     LCD_D7 -> G4                 LCD_D12 -> R4 

    LCD_D2 -> B5                     LCD_D8 -> G5                 LCD_D13 -> R5

    LCD_D3 -> B6                     LCD_D9 -> G6                 LCD_D14 -> R6

    LCD_D4 -> B7                     LCD_D10 -> G7               LCD_D15 -> R7

x 出现错误。请重试或与管理员联系。