This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教6678如何让不同的核运行不同的代码?



亲爱的大牛们:

我遇到的问题是这样的,在编写6678程序的过程中,希望将core0作为主处理器,core1-7作为从处理器,由于完成的功能不相同,代码也是不一样的,当然,可以通过在程序中加各种不同逻辑达到目的,但是很繁琐,所以希望在调试和固化的过程中在core0和core1-7运行不同的程序,有没有具体的调试过称和固化过程在不同核运行不同程序的方法,请指教。

  • 亲爱的大牛们: 我遇到的问题是这样的,在编写6678程序的过程中,希望将core0作为主处理器,core1-7作为从处理器,由于完成的功能不相同,代码也是不一样的,当然,可以通过在程序中加各种不同逻辑达到目的,但是很繁琐,所以希望在调试和固化的过程中在core0和core1-7运行不同的程序,有没有具体的调试过称和固化过程在不同核运行不同程序的方法,请指教。

  • 在ccs下调测的时候建立主从两个工程,分别编译生成out文件,然后分别load到多个core上即可,mcsdk中的image process demo就是一个这样的例子,里面有主从两个工程,安装mcsdk后可以找到这个例子C:\ti\mcsdk_2_01_02_06\demos\image_processing

  • 多谢,问题已经解决。