This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AM335x系列是硬件Pin to Pin兼容、软件兼容的。
你用的是独立的电源解决方案,还是某个电源管理芯片?跑Linux吗?SDK版本呢?
我用的是TPS65910A31电源管理芯片,跑的是linux3.2.0,SDK6.0版本,谢谢您的回答
这个是可以的,这个版本支持PG2.1,关于65910部分的driver也是完善的,不需要做改动。
ps:你可以参考arch/arm/mach-omap2/opp3xxx_data.c这个文件,里面描述了怎么定义出max frequency的,初始化可用的OPP列表。
Steven Liu 说:这个是可以的,这个版本支持PG2.1,关于65910部分的driver也是完善的,不需要做改动。
ps:你可以参考arch/arm/mach-omap2/opp3xxx_data.c这个文件,里面描述了怎么定义出max frequency的,初始化可用的OPP列表。
我补充一点,电路上有一个地方需要注意:
10. [PG2.1兼容设计] For the EXTINTn signal revise compatible design, please refer the PMIC_INT part in beaglebone Schmatic sheet 2 of 11, the inverter of SN74LVC2G00DCU should be removed and the R10 should be added for PG2.1.
主要是要确认下系统有没有用到外部中断,另外如果电源用的是分立的,需要调整VDD_MPU
我使用的是独立电源供电的,VDD_MPU这个电压已经更改为1.287V(在1G电压范围内)但是也只能跑300M,请问硬件上还需要更改什么地方吗