This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用ipnc_rdk 5.1.0版本TCP发送CPU占用率高



使用2.6.18内核TCP发送4Mbps码流的视频流,CPU占用率只有8%-10%,但是使用ipnc_rdk 5.1.0中的2.6.37内核,发送相同码流的视频流,CPU占用率达到16%-18%左右。

请问你们测试有没有出现这个问题?这个问题需要怎么样解决?谢谢