This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127的DDR3芯片



用的是爱普罗的方案,以前的芯片是MT41J128M16HA-125,现在停产了。厂家说的替代型号是MT41K128M16HA-125.所以就改成上MT41K了。

之前在这个板子上我用的是MT41J,什么都调好了,1stboot 杠杠的。现在换了MT41K,连1stboot都进不去。

不知道是什么原因,请帮忙分析一下。谢谢了。

  • 确认一下DDR颗粒的手册,是否时序参数有变化,最好把DDR3的leveling重新做一下,另外可以先试试仿真器能不能连上。

  • DDR leveling的链接: http://processors.wiki.ti.com/index.php?title=TI814x-DDR3-Init-U-Boot&redirect=no

  • 您好,Louis。

    按您的提议,

    这是我从板子上运行

    DDR3_SlaveRatio_ByteWiseSearch_TI814x.out后得到的结果

    Enter 0 for DDR Controller 0 & 1 for DDR Controller 1
    0
    DDR START ADDR=0x80000000

    Enter the Seed Read DQS Gate Ratio Value in Hex to search the RD DQS Gate Window
    0xa5

    Enter the Seed Read DQS Ratio Value in Hex to search the RD DQS Ratio Window
    0x34

    Enter the Seed Write DQS Ratio Value in Hex to search the Write DQS Ratio Window
    0x13
    Enter the input file Name
    Ti814x_Ratio_values
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE
    WR DATA RATIO MAXIMUM VALUE DIDN'T CONVERGE
    WR DATA RATIO MINIMUM VALUE DIDN'T CONVERGE
    *********************************************************
    Byte level Slave Ratio Search Program Values
    *********************************************************
    BYTE3 BYTE2 BYTE1 BYTE0
    *********************************************************
    Read DQS MAX 0 20000007 0 0
    Read DQS MIN 33 0 0 0
    Read DQS OPT 80000019 10000003 0 0
    *********************************************************
    Read DQS GATE MAX 0 0 0 0
    Read DQS GATE MIN 0 0 0 0
    Read DQS GATE OPT 0 0 0 0
    *********************************************************
    Write DQS MAX 0 14 0 0
    Write DQS MIN 0 0 0 0
    Write DQS OPT 0 a 0 0
    *********************************************************
    Write DATA MAX 0 0 0 0
    Write DATA MIN 0 0 0 0
    Write DATA OPT 0 0 0 0
    *********************************************************

    ===== END OF TEST =====

    这个很不好理解。

  • 刚才百度了一下,看到有人提到说MT41J和MT41K的初起不一样,不知道初起是指的什么,在ti814x ddr3的文件里怎么调。

  • 你仔细对比一下J和K的时序参数看看是不是完全一样的。

    时序参数不同的话对DDR时序的配置就是不同的。 Leveling是在时序配置的前提下进一步优化稳定性的手段。

    你的打印指出DDR leveling不能收敛,可能是xls里面的配置有误导致seed初始值不正确,或者DDR时序寄存器不对导致。

    再者, 请问你的情形是全部参数不能收敛,还是部分参数不能。

    如果是后者,请用收敛完毕的参数替代为新的seed填入,重新leveling,这样可能可以进一步帮助收敛其他的值。

  • 你好,请问你最后有没有解决问题?我现在的情况和你一样,用的是一样的DDR3