1.问一下串口的serial_in seril_out函数,用的iowrite8 ioread8函数,请问一下如果连接GPMC总线的话是否需要修改读写函数?改为GPMC读写方式?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
insmod 8250_exar_st16c554.ko
[ 624.628601] ------------[ cut here ]------------
[ 624.633575] WARNING: at fs/sysfs/dir.c:481 sysfs_add_one+0x94/0xb4()
[ 624.640197] sysfs: cannot create duplicate filename '/devices/platform/serial8250.6'
[ 624.648406] Modules linked in: 8250_exar_st16c554(+)
[ 624.653594] Backtrace:
[ 624.656158] [<c0017e34>] (dump_backtrace+0x0/0x10c) from [<c02c9810>] (dump_stack+0x18/0x1c)
[ 624.664978] r6:000001e1 r5:c00ff4b0 r4:c7829ce8 r3:c0429d88
[ 624.670898] [<c02c97f8>] (dump_stack+0x0/0x1c) from [<c003d054>] (warn_slowpath_common+0x54/0x6c)
[ 624.680175] [<c003d000>] (warn_slowpath_common+0x0/0x6c) from [<c003d110>] (warn_slowpath_fmt+0x38/0x40)
[ 624.690063] r8:c7b430e0 r7:c78fa000 r6:c7b430e0 r5:c78fa000 r4:ffffffef
[ 624.696868] r3:00000009
[ 624.699615] [<c003d0d8>] (warn_slowpath_fmt+0x0/0x40) from [<c00ff4b0>] (sysfs_add_one+0x94/0xb4)
[ 624.708862] r3:c78fa000 r2:c0383bbc
[ 624.712615] [<c00ff41c>] (sysfs_add_one+0x0/0xb4) from [<c00ff53c>] (create_dir+0x6c/0xc0)
[ 624.721221] r7:00000000 r6:00000001 r5:bf00b040 r4:c7813310
[ 624.727142] [<c00ff4d0>] (create_dir+0x0/0xc0) from [<c00ff650>] (sysfs_create_dir+0x8c/0xd4)
[ 624.736053] [<c00ff5c4>] (sysfs_create_dir+0x0/0xd4) from [<c01735c4>] (kobject_add_internal+0xa0/0x238)
[ 624.745941] r6:c04470c0 r5:00000000 r4:bf00b040
[ 624.750762] [<c0173524>] (kobject_add_internal+0x0/0x238) from [<c0173a98>] (kobject_add+0x58/0x98)
[ 624.760192] r8:c04470b8 r7:bf00b040 r6:c04470c0 r5:00000000 r4:bf00b040
[ 624.767211] [<c0173a40>] (kobject_add+0x0/0x98) from [<c01c2988>] (device_add+0xa0/0x584)
[ 624.775756] r3:00000000 r2:00000000
[ 624.779479] r6:00000000 r5:bf00b158 r4:bf00b038
[ 624.784332] [<c01c28e8>] (device_add+0x0/0x584) from [<c01c719c>] (platform_device_add+0x114/0x204)
[ 624.793762] [<c01c7088>] (platform_device_add+0x0/0x204) from [<c01c73ec>] (platform_device_register+0x28/0x2c)
[ 624.804290] r7:00000001 r6:00000000 r5:c0455800 r4:bf00b030
[ 624.810211] [<c01c73c4>] (platform_device_register+0x0/0x2c) from [<bf00d014>] (exar_init+0x14/0x1c [8250_exar_st16c554])
[ 624.821746] r4:bf00b2f8 r3:00000000
[ 624.825469] [<bf00d000>] (exar_init+0x0/0x1c [8250_exar_st16c554]) from [<c0008770>] (do_one_initcall+0x44/0x1ac)
[ 624.836212] [<c000872c>] (do_one_initcall+0x0/0x1ac) from [<c006b3d0>] (sys_init_module+0xf8/0x1b04)
[ 624.845733] [<c006b2d8>] (sys_init_module+0x0/0x1b04) from [<c0014700>] (ret_fast_syscall+0x0/0x30)
[ 624.855163] ---[ end trace bf32a16277959dc2 ]---
[ 624.859985] kobject_add_internal failed for serial8250.6 with -EEXIST, don't try to register things with the same name in the same directory.
[ 624.873229] Backtrace:
[ 624.875793] [<c0017e34>] (dump_backtrace+0x0/0x10c) from [<c02c9810>] (dump_stack+0x18/0x1c)
[ 624.884582] r6:c04470c0 r5:ffffffef r4:bf00b040 r3:c0429d88
[ 624.890502] [<c02c97f8>] (dump_stack+0x0/0x1c) from [<c0173734>] (kobject_add_internal+0x210/0x238)
[ 624.899932] [<c0173524>] (kobject_add_internal+0x0/0x238) from [<c0173a98>] (kobject_add+0x58/0x98)
[ 624.909393] r8:c04470b8 r7:bf00b040 r6:c04470c0 r5:00000000 r4:bf00b040
[ 624.916412] [<c0173a40>] (kobject_add+0x0/0x98) from [<c01c2988>] (device_add+0xa0/0x584)
[ 624.924957] r3:00000000 r2:00000000
[ 624.928680] r6:00000000 r5:bf00b158 r4:bf00b038
[ 624.933502] [<c01c28e8>] (device_add+0x0/0x584) from [<c01c719c>] (platform_device_add+0x114/0x204)
[ 624.942962] [<c01c7088>] (platform_device_add+0x0/0x204) from [<c01c73ec>] (platform_device_register+0x28/0x2c)
[ 624.953460] r7:00000001 r6:00000000 r5:c0455800 r4:bf00b030
[ 624.959381] [<c01c73c4>] (platform_device_register+0x0/0x2c) from [<bf00d014>] (exar_init+0x14/0x1c [8250_exar_st16c554])
[ 624.970825] r4:bf00b2f8 r3:00000000
[ 624.974548] [<bf00d000>] (exar_init+0x0/0x1c [8250_exar_st16c554]) from [<c0008770>] (do_one_initcall+0x44/0x1ac)
[ 624.985260] [<c000872c>] (do_one_initcall+0x0/0x1ac) from [<c006b3d0>] (sys_init_module+0xf8/0x1b04)
[ 624.994812] [<c006b2d8>] (sys_init_module+0x0/0x1b04) from [<c0014700>] (ret_fast_syscall+0x0/0x30)
insmod: can't insert '8250_exar_st16c554.ko': File exists
这个问题已经解决了,是由于8250_exar_16c554.c文件中的地址类型错误引起的要用mapbase.
insmod 8250_exar_st16c554.ko
[ 23.651458] Unhandled fault: external abort on non-linefetch (0x008) at 0xc88c0009
[ 23.659393] Internal error: : 8 [#1]
[ 23.663146] Modules linked in: 8250_exar_st16c554(+)
[ 23.668365] CPU: 0 Not tainted (3.2.0 #37)
[ 23.673004] PC is at mem_serial_in+0x18/0x24
[ 23.677490] LR is at serial8250_config_port+0x104/0xbe8
[ 23.682952] pc : [<c01b79a0>] lr : [<c01ba510>] psr: 40000093
[ 23.682952] sp : c78fbb58 ip : c78fbb68 fp : c78fbb64
[ 23.694976] r10: c046d2f8 r9 : c046d2f4 r8 : 00000000
[ 23.700439] r7 : 20000013 r6 : fffffffe r5 : 00000001 r4 : c046d2f8
[ 23.707275] r3 : c88c0008 r2 : 00000001 r1 : 00000001 r0 : c046d2f8
[ 23.714111] Flags: nZcv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
[ 23.721649] Control: 10c5387d Table: 87bd4019 DAC: 00000015
[ 23.727661] Process insmod (pid: 1234, stack limit = 0xc78fa2f0)
[ 23.733947] Stack: (0xc78fbb58 to 0xc78fc000)
[ 23.738525] bb40: c78fbba4 c78fbb68
[ 23.747070] bb60: c01ba510 c01b7994 c7a48e00 00000000 c78fbb94 c78fbb80 c0174a60 c0446940
[ 23.755645] bb80: c046d2f8 c7a48e00 c7a48e30 00000004 c046d2f4 c046d2f8 c78fbc34 c78fbba8
[ 23.764190] bba0: c01b72a8 c01ba418 c78fbbc4 c78fbbb8 c01c1948 c0173264 c78fbbdc c78fbbc8
[ 23.772766] bbc0: c01c27dc c01c1938 00000003 c7a48a00 c78fbbfc c78fbbe0 c01c2848 c01c27b8
[ 23.781341] bbe0: c04297f0 00400040 c7b77480 c046d2f8 c78fbc0c c78fbc00 c019c80c c01c281c
[ 23.789886] bc00: c78fbc34 c78fbc10 c01b52cc c046d2f8 00000004 c78fbc78 c0446940 00000004
[ 23.798461] bc20: c046d2f4 c046d2f8 c78fbc64 c78fbc38 c01b9cd0 c01b71ac 00000000 bf0001bc
[ 23.807006] bc40: 00000001 bf000038 c78fbc78 00000080 0000010b 00000000 c78fbd3c c78fbc68
[ 23.815582] bc60: c02c6c18 c01b9b34 c7b3e5e0 c78fbcf0 c7b3e0e0 c78fbcf0 00000000 00000000
[ 23.824127] bc80: 00000000 00000000 00000000 00000000 00000000 00000007 00000081 00708000
[ 23.832702] bca0: 00000000 00020000 00000000 00000000 00000000 00000000 00000000 00000000
[ 23.841278] bcc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 23.849822] bce0: 00000000 00000000 90000000 00000000 00000000 00000000 00000000 00000000
[ 23.858398] bd00: 00000000 00000008 bf000038 00000000 00000000 00000000 bf000038 c046db80
[ 23.866943] bd20: c0452d88 c04469dc c04470b8 c046db5c c78fbd4c c78fbd40 c01c6acc c02c6b40
[ 23.875518] bd40: c78fbd7c c78fbd50 c01c54d8 c01c6ab8 c78fbd7c c78fbd60 c01c6ea4 c04469dc
[ 23.884063] bd60: bf000038 c01c5794 00000000 c04470b8 c78fbd94 c78fbd80 c01c57d8 c01c542c
[ 23.892639] bd80: bf000038 c78fbd98 c78fbdbc c78fbd98 c01c4134 c01c57a0 c7806f08 c7a41574
[ 23.901214] bda0: bf000038 bf00006c 00000000 bf000040 c78fbddc c78fbdc0 c01c52f4 c01c40d8
[ 23.909759] bdc0: 00000001 bf000038 bf000158 00000000 c78fbdec c78fbde0 c01c4aac c01c5264
[ 23.918334] bde0: c78fbe3c c78fbdf0 c01c2d80 c01c4a8c c01739c4 00000000 00000000 bf000030
[ 23.926879] be00: bf000038 00000001 c78fbe30 c78fbe18 c01c1b14 00000000 bf000030 bf000038
[ 23.935455] be20: 00000001 c7bb8740 0000010b 00000001 c78fbe5c c78fbe40 c01c719c c01c28f4
[ 23.944000] be40: bf000030 c0455800 00000000 00000001 c78fbe74 c78fbe60 c01c73ec c01c7094
[ 23.952575] be60: 00000000 bf0002f8 c78fbe84 c78fbe78 bf002014 c01c73d0 c78fbee4 c78fbe88
[ 23.961151] be80: c0008770 bf00200c 00000001 c7bb8740 c78fbeb4 c78fa000 bf002000 00000000
[ 23.969696] bea0: c7ae6b80 00000000 c78fbed4 c78fbeb8 bf0002f8 bf0002b0 0000001c bf0002f8
[ 23.978271] bec0: bf0002b0 0000001c 00000001 c7bb8740 0000010b 00000001 c78fbfa4 c78fbee8
[ 23.986816] bee0: c006b3d0 c0008738 bf0002bc c78102c0 c7b87e48 00000000 c006a194 000a2008
[ 23.995391] bf00: c887d4e8 c887d4e8 c78fa000 00000025 bf0003d0 bf0002bc c78fbf34 c887d000
[ 24.003967] bf20: 00000d1b c887d6a0 c887d5e7 c887dc10 c7bb8880 000003e4 000003f4 00000000
[ 24.012512] bf40: 00000000 00000011 00000012 00000009 00000006 00000004 00000000 00000000
[ 24.021087] bf60: 00000000 00000000 00000000 00000000 00000000 c03bdb6c 00000000 be98bea6
[ 24.029632] bf80: 000a2018 000a2008 00000080 c00148a8 c78fa000 00000000 00000000 c78fbfa8
[ 24.038208] bfa0: c0014700 c006b2e4 be98bea6 000a2018 000a2018 00000d1b 000a2008 00000000
[ 24.046752] bfc0: be98bea6 000a2018 000a2008 00000080 000a0aa4 0000cf20 be98bd18 00000000
[ 24.055328] bfe0: 400edd34 be98bc98 0001b184 400edd44 20000010 000a2018 00000000 00000000
[ 24.063873] Backtrace:
[ 24.066467] [<c01b7988>] (mem_serial_in+0x0/0x24) from [<c01ba510>] (serial8250_config_port+0x104/0xbe8)
[ 24.076385] [<c01ba40c>] (serial8250_config_port+0x0/0xbe8) from [<c01b72a8>] (uart_add_one_port+0x108/0x38c)
[ 24.086761] [<c01b71a0>] (uart_add_one_port+0x0/0x38c) from [<c01b9cd0>] (serial8250_register_port+0x1a8/0x268)
[ 24.097351] [<c01b9b28>] (serial8250_register_port+0x0/0x268) from [<c02c6c18>] (serial8250_probe+0xe4/0x14c)
[ 24.107727] [<c02c6b34>] (serial8250_probe+0x0/0x14c) from [<c01c6acc>] (platform_drv_probe+0x20/0x24)
[ 24.117462] [<c01c6aac>] (platform_drv_probe+0x0/0x24) from [<c01c54d8>] (driver_probe_device+0xb8/0x2dc)
[ 24.127502] [<c01c5420>] (driver_probe_device+0x0/0x2dc) from [<c01c57d8>] (__device_attach+0x44/0x48)
[ 24.137237] r8:c04470b8 r7:00000000 r6:c01c5794 r5:bf000038 r4:c04469dc
[ 24.144287] [<c01c5794>] (__device_attach+0x0/0x48) from [<c01c4134>] (bus_for_each_drv+0x68/0x94)
[ 24.153656] r5:c78fbd98 r4:bf000038
[ 24.157409] [<c01c40cc>] (bus_for_each_drv+0x0/0x94) from [<c01c52f4>] (device_attach+0x9c/0xc0)
[ 24.166595] r7:bf000040 r6:00000000 r5:bf00006c r4:bf000038
[ 24.172546] [<c01c5258>] (device_attach+0x0/0xc0) from [<c01c4aac>] (bus_probe_device+0x2c/0x48)
[ 24.181732] r6:00000000 r5:bf000158 r4:bf000038 r3:00000001
[ 24.187683] [<c01c4a80>] (bus_probe_device+0x0/0x48) from [<c01c2d80>] (device_add+0x498/0x584)
[ 24.196807] [<c01c28e8>] (device_add+0x0/0x584) from [<c01c719c>] (platform_device_add+0x114/0x204)
[ 24.206268] [<c01c7088>] (platform_device_add+0x0/0x204) from [<c01c73ec>] (platform_device_register+0x28/0x2c)
[ 24.216827] r7:00000001 r6:00000000 r5:c0455800 r4:bf000030
[ 24.222778] [<c01c73c4>] (platform_device_register+0x0/0x2c) from [<bf002014>] (exar_init+0x14/0x1c [8250_exar_st16c554])
[ 24.234252] r4:bf0002f8 r3:00000000
[ 24.238006] [<bf002000>] (exar_init+0x0/0x1c [8250_exar_st16c554]) from [<c0008770>] (do_one_initcall+0x44/0x1ac)
[ 24.248748] [<c000872c>] (do_one_initcall+0x0/0x1ac) from [<c006b3d0>] (sys_init_module+0xf8/0x1b04)
[ 24.258331] [<c006b2d8>] (sys_init_module+0x0/0x1b04) from [<c0014700>] (ret_fast_syscall+0x0/0x30)
[ 24.267822] Code: e24cb004 e5d0202d e5903004 e1a02211 (e7d30002)
[ 24.274505] ---[ end trace 27588c68e8ff92ef ]---
Segmentation fault
这个已经解决,是由于FPGA引起的。CS只开了一路导致其他三路由于无法取到相应的资源而出现的内核崩溃和段错误。
我看你一直在自问自答啊,能不能把问题出现的描述下,也好做个总结啊
现在有个问题,就是通过FPGA软件分析时序发现一个问题。验证TL16C554a的时序都是正确的,但是到IOR IOW的上升沿后发现没有数据数据。下边是有可能的问题
1.我发现RESET554连到了FPGA上处于高电平,芯片处于复位状态,已经把这个27管脚RESET拉底了
2.经过1步还发现不是这个问题引起的,又仔细对了一下,时序是周建给出的那个时序。这个我希望重新CHECK一下。
3.后来测量了电源,时钟发现都没有问题。
4.如果时序正常的情况下,芯片又不处于复位状态,供电和晶振都正常工作,请问为什么读写数据老是总线上的数据呢?
我是这样验证的
我看16c554的datasheet,reset信号应该是高有效,也就是先置低,然后置高1ms,然后再置低
周建,其实RESET并不影响实际的芯片使用情况。上周我发送时序图给了TL16C554A的人,还有FPGA的时序,上面标注的很清楚了。FPGA有数据输出TL16C554没有。现在时序是对的。但TL16C554不工作。RESET部分已经改了,但是还是无法使用,供电部分还有晶振都是正常的。已经测量过。