This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
环境:win7 32为位;CCS3.1,Flashburn2.8 ,板子C6713B,Flash:4M,8bit
另外环境变成CCS3.3PLA和对应的Flashburn:setup_FlashBurnDSK_v311.exe也出现这样的问题
Shoukuan Wang 说:另外环境变成CCS3.3PLA和对应的Flashburn:setup_FlashBurnDSK_v311.exe也出现这样的问题
也是在win7操作系统下吗?
另外用flashburn烧写插件时,CCS也是要打开的。
在XP、Win7系统都试装了Flash Burn 3,但是都是出现Failed to create Code Composer instance,打开CCS也不行(CCS5.3版本),怎么解决?
另外,用Flash Burn 4软件下,FBTC文件从哪里下载?(开发板是6455DSK)