1、请问DM642可以实现两路D1格式的mpeg-2的编码吗?要求具有实时性
2、对于1路时频频输入来说,进行mpeg-2的编码,DM6446比DM642能提高多少速度?DM6446比DM642的优势在哪里,视频加速器对于视频的处理有多大的作用,能将速度提高几倍?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、请问DM642可以实现两路D1格式的mpeg-2的编码吗?要求具有实时性
2、对于1路时频频输入来说,进行mpeg-2的编码,DM6446比DM642能提高多少速度?DM6446比DM642的优势在哪里,视频加速器对于视频的处理有多大的作用,能将速度提高几倍?
你好,
Q2:TI官方没有mpeg2enc,支持的视频算法见:http://software-dl.ti.com/dsps/dsps_public_sw/codecs/DM644X/index_FDS.html。如果需要mpeg2enc,应该需要问第三方购买。
你是什么应用啊,还在用mpeg2?
项目需求,具体的方案还在讨论中,我们自己做的mpeg-2的算法的移植,基于DM642的,一路视频输入,但是还没有达到实时性,而根据要求是两路视频输入然后进行MPEG-2压缩,我现在再找有没有更好的芯片,可以支持至少两路视频输入的,性能比DM642好的?
项目需求,我们已经实现了在DM642上的mpeg-2的移植,一路视频输入,但是还未达到25fps,现在也就15fps,所以想问一下,DM642能不能支持两路D1格式的mpeg2的压缩编码,或者说我想要实现两路D1格式的mpeg-2编码,要求实时性,有什么更好的解决方案吗?
你的编码算法是在DSP上跑的?
要多路实时编码的话建议用新一些的芯片。新的DM81xx芯片都是能做到的
是的,因为DM642只有dsp核,所以包括驱动和传输还有算法之前都是在dsp上跑的。
还想请问一下,在DM81XX这类芯片上的开发周期长不长,比如DM8168?