This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6416的TCP核的使用问题,求大神帮忙解答。



问题1,:我看spra749b中3.2.1节的内容发现要求输入数据的格式是SIIII.FFF即8bits的形式5Q3格式输入,S为符号位,IIII为4位代表整型的比特,FFF为小数点位,此数的动态范围应该是[-16, 15.875],而TI提供的该文档中确实[-32, 31.875],我不明白是如何计算得到的?5bit有符号数据的动态范围不应该是[-16,15]吗?到底是我理解出了问题?还是应该数据怎么处理的? 5Q3的范围到底是多少?

问题2:承接上面的问题,我对接收到的不加噪的软数据进行归一化后,乘以2^7后化为SIIII.FFF形式的8bits的16进制数据送入TCP核,发现译码是完全正确的。可问题来了,同样的过程,我加噪声后再将处理后的数据送入TCP译码出现大量错误,这是为什么?参数都没有改变,为何加了噪声后就不正确了呢,使用的工程是在论坛上下载的TcpStandaloneProcessing.prj,SA模式。

到底是哪一块出现问题呢?我怀疑我对加噪的数据进行归一化乘以2^7后数据在【-128,127】之间换算成8bits进行TCP核中数据处理这一款是否我理解的有问题,可如果我理解的有问题为何不加噪的情况下我尝试了N组数据都是译码完全正确的,希望大神帮我提供思路。